Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Transformer part number Issue

Posted on August 27, 2015 at 15:25Hello ,         I am designing a battery charger using this IC ALTAIR05T-800 but wurth transformer part no. is not mention as if i search on wurth site it doesnt exit.Plz provide me the transformer part no. and whic...

STM8 internal EEPROM and Toolchain

Posted on July 16, 2015 at 10:25Hi all! ST Visual Development Raisonance Debugger Cosmic Compiler The following problem: It seems that the internal EEPROM is erased every time the debugger writes new software into the controller. Is it possible to ...

STM8 HWI2C and ClockStretching

Posted on August 27, 2015 at 10:17Hi @ all! I'm using the HWI2C interface as a I2c slave. Now I need to activate clock stretching on the SCL line to tell the master that the device is busy. Is there a possibility to activate clock stretching (SCL to...

STM8S Reload Watchdog Timer During Halt Mode

Posted on August 24, 2015 at 18:43Hey guys, I am using an STM8S003F3 and am trying to implement a watchdog timer. I have been using the IWDG functions from the standard peripheral library and it seems to work, but once I enter HALT mode I can't rese...

cfleck by Associate II
  • 1046 Views
  • 0 replies
  • 0 kudos

TIM2 interrupt at 100 kHz frequency

Posted on August 14, 2015 at 08:39 Hello! I have a little question about STM8S interrupt controller. I'm using IAR and the following code isn't quite clear for me. INTERRUPT_HANDLER(TIM2_UPD_OVF_BRK_IRQHandler, 13) { //Here ar...

wir2ozz by Associate
  • 1116 Views
  • 0 replies
  • 0 kudos

STM8L151G4U6 EEPROM maxiam programming time

Posted on August 12, 2015 at 08:11Hello ST Experts, Can you please advise the maximum programming time of the STM8L151G4U6 MCU EEPROM. The datasheet only mention the typical programming time. The maximum programming time is related to watch dog sett...

sinclair by Associate
  • 918 Views
  • 0 replies
  • 0 kudos

List of STM8S opcodes

Posted on July 13, 2013 at 06:51I have looked but can't find a ''complete listing of the op-codes for this MCU.  I'm using the STM8S-Discovery to teach my grand-kids programming, starting at the very basic machine language, then to assembler and the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.