Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using stm8af52AA controller and L9950 as slave and i am doing the SPI communication.please send me the source code .

Posted on August 11, 2017 at 07:38I am trying to communicate the stm8af52AA controller with L9950 slave ic but slave is not responding  properly.In datasheet they mentioned 24 clock cycle but my controller is generating  16 clock please help me

Controller reset

Posted on July 24, 2017 at 11:11I know it is a common question but still we cannot get rid of it. We are using stm8s003f3 in our project. An ac motor is switched ON and OFF by a 12V relay (using timer).The controller frequently resets itself when a ...

Cann't enter capture interrupt subroutine

Posted on August 08, 2017 at 14:25hi all, I have recently tried the official code according to the application note AN2822: STM8S and STM8A high speed internal oscillator calibration. Since I use STM8S003k3 MC, I modified the code from timer 3 to ti...

Lei Sun by Associate II
  • 1109 Views
  • 0 replies
  • 0 kudos

STM8L051F3 RTC Issue

Posted on August 02, 2017 at 23:33I'm struggling to initialize the RTC on an STM8L051F3 microcontroller. I've used the exact code below on an STM8L151K6 microcontroller with no issues. The code hangs waiting for the LSI clock to be ready. Interrupts...

Brian1 by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

stm8l151c8 Interrupt is not working

Posted on July 29, 2017 at 15:58Hi,I'm using stm8l151c8 controller, I'm trying to get an interrupt from PB0 but it's not working, here is my code:&sharpinclude 'stm8l15x_conf.h'&sharpinclude 'main.h'uint8_t __IO BlinkSpeed = 0;static __IO uint32_t T...

Power MOSFET Simulation Model

Posted on July 28, 2017 at 17:50 Hello, I'm trying to simulate STP55NF You can download its model here: http://www.st.com/en/power-transistors/stp55nfhtml. The pin 1,2, and 3 should be gate, drain, and source respectively. I connected a circ...

0690X00000607fCQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.