2017-07-24 2:11 AM
I know it is a common question but still we cannot get rid of it. We are using stm8s003f3 in our project. An ac motor is switched ON and OFF by a 12V relay (using timer).
The controller frequently resets itself when a relay is tripped ON or OFF. We used pf on the controller pin, pulled up the NRST pin with a 10K and a pf, used 7805 instead of lm1117, and tried a few other things, but couldn't succeed.It would be a great relief for us if anybody can provide solution for it.THANK YOU.2017-07-29 4:45 PM
Add a tvs,you wiil have an amazing discovery.
2017-07-29 7:25 PM
What is 'pf' in this context? You've tried what? You have a schematic of what you've implemented?
Do you have adequate bulk capacitance on either side of the regulator?
2017-07-30 12:53 AM
just add a tvs
in front of the power supply of mcu,in my sch the NRST pin is 100nF,but the most problem is EFT when the AC motor on or off.
2017-08-08 12:57 AM
We have used 104 pf.
Yes. We have added adequate capacitance on both sides.
2017-08-08 7:21 AM
Ok. But can you suggest the value of tvs? I think 9 to 19V tvs is the most widely used one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.