2017-08-08 5:25 AM
hi all, I have recently tried the official code according to the application note AN2822: STM8S and STM8A high speed internal oscillator calibration. Since I use STM8S003k3 MC, I modified the code from timer 3 to timer 1 channel 1. But I found that I could not enter the timer1 capture interrupt subroutine (the capture interrupt subroutine is never called), although I have checked the necessary registers' values using debug mode and all registers are correctly set.
I have tried as mentioned in AN2822 the signal generater input with 50Hz frequency on the PC1 port (TIM1_CH1) but it seems that the rising edge of the input signal is never captured by STM8S003k3.
I have also edited a simple example for the overflow interrupt and capture interrupt of timer1:
The main function:
&sharpinclude 'stm8s_lib.h'
&sharpinclude 'stdlib.h'u16 cntr;
u16 LEDflag; main(){ GPIO_DeInit(GPIOC); GPIO_Init(GPIOC, GPIO_PIN_5, GPIO_MODE_OUT_PP_LOW_FAST); GPIO_Init(GPIOC, GPIO_PIN_6, GPIO_MODE_OUT_PP_LOW_FAST); GPIO_Init(GPIOC, GPIO_PIN_7, GPIO_MODE_OUT_PP_LOW_FAST); GPIO_WriteHigh(GPIOC, GPIO_PIN_5); GPIO_WriteHigh(GPIOC, GPIO_PIN_6); GPIO_WriteHigh(GPIOC, GPIO_PIN_7); GPIO_Init(GPIOC, GPIO_PIN_1, GPIO_MODE_IN_FL_NO_IT); cntr = 0; LEDflag = 0; CLK_DeInit(); CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV1); // Clock divider to HSI/1 CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1); // Fcpu division factor: /1 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, TIM1_ICPSC_DIV8, 0x03);TIM1_UpdateRequestConfig(TIM1_UPDATESOURCE_REGULAR); // Update interupt request is sent only when the counter overflow
TIM1_UpdateDisableConfig(DISABLE); // Update Event Enable TIM1_ClearITPendingBit(0xFF); // Clear all pending interupts TIM1_ITConfig(TIM1_IT_CC1, ENABLE); // Capture/Compare 1 Interrupt Enable TIM1_ITConfig(TIM1_IT_UPDATE, ENABLE); // Update Interrupt Enable TIM1_Cmd(ENABLE); // enable counter while(1){}; }stm8s_it.c:
extern u16 cntr;
extern u16 LEDflag;@near @interrupt void TIM1_UPD_OVF_TRG_BRK_IRQHandler(void)
{ TIM1_ClearITPendingBit(TIM1_IT_UPDATE); // clear all interupt flagsreturn;
}
@near @interrupt @svlreg void TIM1_CAP_COM_IRQHandler (void)
{ GPIO_WriteLow(GPIOC, GPIO_PIN_5); if ( TIM1_GetFlagStatus(TIM1_FLAG_CC1) == SET ) { GPIO_WriteLow(GPIOC, GPIO_PIN_5); cntr++; if (cntr > 10) { cntr = 0; if (LEDflag == 0) { //toggle LED C6 LEDflag = 1; GPIO_WriteLow(GPIOC, GPIO_PIN_6); } else { LEDflag = 0; GPIO_WriteHigh(GPIOC, GPIO_PIN_6); } }} else { GPIO_WriteLow(GPIOC, GPIO_PIN_7);}
TIM1_ClearITPendingBit(TIM1_IT_CC1);return;}
The interrupt vector stm8_interrupt_vector.c
...
(void @near (*)())0x8200,
TIM1_UPD_OVF_TRG_BRK_IRQHandler,/* irq11 - TIM1 Update/Overflow/Trigger/Break interrupt */(void @near (*)())0x8200,
TIM1_CAP_COM_IRQHandler, /* irq12 - TIM1 Capture/Compare interrupt */...
I used the standard firmware. I could not get any timer1 channel1 capture interrupt and the capture interrupt subroutine is never entered.
I want to ask if anybody has similar experience on this problem: why the timer1_channel1 rising signal cannot be
captured and the interrupt subroutine cannot be called? I would appreciate if you give me just some hints. Thanks all!
Bo
#stm8s-interrupt #timers-input-captureWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.