Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cosmic compiler and STM8L052R8 error

Posted on January 25, 2018 at 11:06Hello, I'm using STM8L052R8(64KBytes ROM, 4KBytes RAM) and cosmic compiler.I can see as below.#error clnk Debug\dm5xx_stm8l.lkf:14336 (C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\lib\libm.sm8)fmul.o: section...

CS Kim by Associate II
  • 2396 Views
  • 5 replies
  • 0 kudos

EEPROM Write Problem at Power-down

Posted on January 23, 2018 at 21:58Hi,I am using the STEVAL-IHM041V1 demo board to develop my own application. The mcuis STM8S103F3P6. I checked the EEPROM locations to verify that the EEPROM read/writeare fine when the +5V is stable. But I have pro...

Sam Zeng1 by Associate II
  • 2025 Views
  • 2 replies
  • 0 kudos

STM8L151G4U6 PD problom

Posted on February 01, 2018 at 11:11i use stm8l151g4 pd4 to control external ADC converter,when pd4=1,ADC converter start,and pd4=0,ADC converter stop,pd4 initialized as below: PD_DDR_DDR4 = 1;       //PD4- OutputPD_CR1_C14 = 1;          //PD4 - Pus...

Interrupt voltage and current

Posted on January 31, 2018 at 21:55Where do I find (manual and section/table) the voltage required to set external interrupt to low and high and also the minimum and maximum current.  I am looking for this information for the STM8L152C6, so somethin...

FlexLM No such feature exists

Posted on January 29, 2018 at 17:02When I try to compile my project or the standard project, I get the message -clDebug \ -coDebug \ main.c #error cpstm8 C: \ Program Files (x86) \ COSMIC \ CXSTM8_32K \ Hstm8 \ mods0.h: 1 FlexLM No such feature exis...

Ivan Yu by Associate
  • 1707 Views
  • 1 replies
  • 0 kudos

stm8s TIM1 PWM not working

Posted on April 18, 2016 at 14:20Hi,I'm trying to operate TIM1 on STM8S003F3P6, I am using the standard peripheral library code, but I am only able to produce pwm on TIM1_CH3 (PC3) pin, the other pins do not produce any waveforms at all. I'm sure th...

udilevy by Associate II
  • 3269 Views
  • 2 replies
  • 0 kudos

Can someone break down this line of code for me? #define TIM1_PSCRH (*(volatile uint8_t *)0x5260)

Posted on January 23, 2018 at 23:47&sharpdefine TIM1_PSCRH (*(volatile uint8_t *)0x5260)I understand that now when I set TIM1_PSCRH = <some 8 bit value> that the Timer 1 Prescaler High Byte register will be set because it is located at address 0x526...

Error during compiling

Posted on January 24, 2018 at 08:07I am getting an error while compiling the file.Can any one please help me out.sdcc -lstm8 -mstm8 --out-fmt-ihx delay.c?ASlink-Warning-Undefined Global '_GPIO_Init' referenced by module 'delay'?ASlink-Warning-Undefi...

STM8L051F3 Halt Mode 300-400nA

Posted on January 24, 2018 at 12:10Hi,   I looking to achieve lowest power consumption in halt mode. Datasheet says we can achieve 350nA in halt mode. I am able to achieve 195 uA(micro Amp) at 1.8V.. I have written simple test code. FYI i am adding ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.