2018-02-01 2:11 AM
i use stm8l151g4 pd4 to control external ADC converter,when pd4=1,ADC
converter
start,and pd4=0,ADCconverter stop,pd4 initialized as below:
PD_DDR_DDR4 = 1; //PD4- Output
PD_CR1_C14 = 1; //PD4 - Push-pull
PD_CR2_C24 = 0; //PD4 - Output speed up to 2 MHz...
PD_ODR_ODR4 = 1; //ADC start convert
...
PD_ODR_ODR4 = 0; //ADC stop convert
but when PD_ODR_ODR4 = 1, the PD4 pin is still 0,why?
btw:The circuit and the program work good at the beginning.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.