2018-01-24 3:10 AM
Hi,
I looking to achieve lowest power consumption in halt mode.
Datasheet says we can achieve 350nA in halt
mode. I am able to achieve195 uA(micro Amp) at 1.8V
.. I have written simple test code. FYI i am adding my code below which is written in STVD IDE and attached project folder also.How can i achieve 350nA? Plz help me
Code:main.c
/* Includes ------------------------------------------------------------------*/
&sharpinclude 'stm8l15x.h'/* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*//* Private function prototypes -----------------------------------------------*/void Delay (uint16_t nCount);/* Private functions ---------------------------------------------------------*/void GPIO_LowPower_Config(void)
{/* Port A in output push-pull 0 */
GPIO_Init(GPIOA, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3 ,GPIO_Mode_Out_PP_Low_Slow); /* Port B in output push-pull 0 */ GPIO_Init(GPIOB, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow);/* Port C in output push-pull 0 except Button pins */
GPIO_Init(GPIOC, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6, GPIO_Mode_Out_PP_Low_Slow);/* Port D in output push-pull 0 */
GPIO_Init(GPIOD, GPIO_Pin_0, GPIO_Mode_Out_PP_Low_Slow);}
void Halt_Init(void)
{/* Set STM8 in low power */ PWR->CSR2 = 0x2; /* Stop RTC Source clock */ CLK_RTCClockConfig(CLK_RTCCLKSource_Off, CLK_RTCCLKDiv_1); /* Stop clock RTC and LCD */ CLK_PeripheralClockConfig(CLK_Peripheral_RTC, DISABLE);}void main(void)
{ GPIO_LowPower_Config();/* Set GPIO in low power*/ while (1) { Halt_Init(); sim(); Delay(10); halt(); }}void Delay(__IO uint16_t nCount){ /* Decrement nCount value */ while (nCount != 0) { nCount--; }}&sharpifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* Infinite loop */ while (1) {}}&sharpendif#stm8l051f3-350na-halt-modeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.