Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pspice model for power factor controller L6563

Posted on April 05, 2010 at 06:22Dear friends,                       I am in need of Pspice model for power factor controller L6563. please post ur suggestion for getting the same or is any other way to simulate the power factor correction? #ede...

jogy_geo by Associate
  • 2062 Views
  • 3 replies
  • 0 kudos

Can't include drivers

Posted on July 02, 2018 at 15:59Hello everyone i'm using system workbench for STM32 (sw4stm32) eclipse based IDE for my development. I'm trying to separate libraries and main file in two different projects but both are in same workspace. So I want f...

STM8S001J3 UART remap

Posted on January 05, 2018 at 10:14HiSTM8S001J3 There is a problem with UART communication.If PIN8 is used without remapping tx, it works well.If tx is remapped and used as PIN5, the following code will not work.void UART1_init(void){    CLK->CKDIVR...

TIM2_CH1/2 remaping on STM8L051F3

Posted on June 30, 2018 at 13:52Hi everybody!I have a problem with the TIM2_CH1 output pin on STM8L051F3 (20-pin TSSOP).In the datasheet (Rev. 3), there are 2 options for the TIM2_CH1 signal: PB0 (pin 10) and PC5 (pin 1); but I cannot find anything ...

Board Bring-up with STM8L051F3

Posted on June 26, 2018 at 13:12Hi,I need your help to find out the root cause of my issue,please help to check the issue, thankful for your support in advance,thanks.issue,when trying to do bring-up new board, we can't control any port related with...

Not able to change the IWDG timeout in STM8S003

Posted on June 28, 2018 at 10:44Hi everyone, I am trying to enable IWDG timer and working for me. but i am not able to change the iwdg timeout, it always ~8ms. I am using HSI CLOCK(16MHz) and referring the Example code provided by ST .I think the ma...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.