2018-06-28 1:44 AM
Hi everyone, I am trying to enable IWDG timer and working for me. but i am not able to change the iwdg timeout, it always ~8ms. I am using HSI CLOCK(16MHz) and referring the Example code provided by ST .
I think the maximum iwdg timeout is 1 sec for STM8S003. Am I right??
here is my source code. I am configuring 250ms IWDG timeout. but getting IWDG timeout is < 8ms. please help me to figure out the issue.
LsiFreq=128000; //128khz
void main(void)
{
/* Configures clocks */
clock_configuration();IWDG_Config();
while(1)
{
/* Reload IWDG counter */
IWDG_ReloadCounter();}
}
void IWDG_Config(void)
{ /* IWDG timeout equal to 250 ms (the timeout may varies due to LSI frequency dispersion) */ /* Enable write access to IWDG_PR and IWDG_RLR registers */ IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable); /* IWDG counter clock: LSI/128 */ IWDG_SetPrescaler(IWDG_Prescaler_128; /* Set counter reload value to obtain 250ms IWDG TimeOut. Counter Reload Value = 250ms/IWDG counter clock period = 250ms / (LSI/128) = 0.25s / (LsiFreq/128) = LsiFreq/(128 * 4) = LsiFreq/512 */ IWDG_SetReload((uint8_t)(LsiFreq/512)); /* Reload IWDG counter */ IWDG_ReloadCounter(); /* Enable IWDG (the LSI oscillator will be enabled by hardware) */ IWDG_Enable();}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.