2018-07-02 11:13 PM
Hi
I use STM8S-Discovery Board with STM8S105C6 and ST Visual Develop v4.3.10, Windows 10.
If I use command ADDW or SUBW this way:
------------------------------------------------------------------------------
Example 1
ldw X,&sharp400
;Load 400 into Xaddw X,&sharp100
;Add direct 100 to word Xtest cpw X,&sharp500
;Compare X with 500jreq test
;Jump to 'test' if X=500------------------------------------------------------------------------------
it works properly. The content X is 500.
But if I do this
------------------------------------------------------------------------------
Example 2
k equ $0365
;RAM register is called kmov k,&sharp100
;Move 100 into kldw X,&sharp400
;Load 400 into Xaddw X,k
;Add k to word Xtest cpw X,&sharp500
;Compare X with 500jreq test
;Jump to 'test' if X=500------------------------------------------------------------------------------
it doesn�t work. The content of X is not 500.
SUBW behave the same way.
According the programming manual PM004 Doc ID 13590 Rev3, page 78 and 152,
Example 2 should actually work. Issue or do I miss something?
Thanks for reply.
Ivan
#addw #subw #stm8s105c6 #basic-arithmetic #issueWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.