Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does is SDCC the DCE optimisation?

Posted on July 14, 2018 at 07:05Hello anyone,When compiling a program including Standard Peripheral Library in the output *.elf file, all unused modules was included. Does is SDCC the dead code elimination optimization and how to activate it?Thanks ...

stm8l051f3 can do for floating operation ????

Posted on July 09, 2018 at 13:57Hello,I have a question as to whether stm8L051F3 can do/calculate the floating operation or not,please help to let me know it,currently I can't check it with printf function, because if using the library with tool opt...

STSW-STM8069 is free to use for product

Posted on July 13, 2018 at 06:22Hi,I would like to develop and sell one of my product using STM8S IC with STSW-STM8069 library from STVD and STVP.is there any licence for that?  if yes ,what is process to get licence for one and how much i have to p...

Hiren M by Associate
  • 2148 Views
  • 2 replies
  • 0 kudos

Datasheet for L9748

Posted on July 09, 2018 at 15:44I have a ECM from my Cherokee 1998 and the injectors are driven by a chip called W990L9748. I need a datasheet for that, i think that  i have one twisted channel on that.

ESD EMI protection for USB OTG

Posted on March 16, 2016 at 10:20Hello ,As per my project requirement, i need to design USB OTG which meets the ESD standard IEC 61000-4-2 level 4) and EMI standard CISPR-11. In ST website i found two categories:1. Common mode filter with ESD protec...

koyala by Associate
  • 1404 Views
  • 1 replies
  • 0 kudos

Stm8l001j3m3 standard library

Posted on July 06, 2018 at 10:05Hi,Where can ı find the standart library for stm8l001j3. The system offers to use the STSW-STM8016 standard peripheral library but this library does not include the stm8l001j3. I need help for this stuation. What are...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.