2016-03-16 2:20 AM
Hello ,
As per my project requirement, i need to design USB OTG which meets the ESD standard IEC 61000-4-2 level 4) and EMI standard CISPR-11. In ST website i found two categories:1. Common mode filter with ESD protection2. EMI filter and ESD protectionBoth claims, same ESD protection levels. So, i am not sure which is used for what and what is the basic difference between them.? Kindly suggest.Regards,Govind. #emi/esd #usb-otg2018-07-11 8:02 AM
Hi,
To solve interference problems, you must understand them. So at first please begin by describing the ways
that RF interference is coupled into equipment and detected. There are several principal mechanisms
at work. You should study this tutorial thoroughly to understand how these things work.
http://audiosystemsgroup.com/RFI-Ham.pdf
http://www.karinya.net/g3txq/chokes/
Hope it helps,
P.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.