Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8 - Unable to use timer2 with interrupt

I am trying to run timer interrupt in STM8 microcontroller. But I am not able to do so.Here is the code snippet. void TIM2_Configuration(void) { TIM2_DeInit(); CLK_PeripheralClockConfig(CLK_PCKENR1_TIM2, ENABLE); TIM2_ARRPreloadConfig(EN...

DPaga by Associate
  • 1690 Views
  • 1 replies
  • 0 kudos

Beginning project to use beCAn on a stm8s208, mere presence of either CAN interrupt vector interferes with TIM4_UPD_OVF_IRQHandler.

No attempt yet to initialize can, just adding entry into interrupt vector table table for either can rx or can tx impacts TIM4_UPD_OVF_IRQHandler. TIM4 will run twice, then never run again.Can interrupts are not enabled yet, can interrupt vector neve...

GOgle by Associate
  • 832 Views
  • 0 replies
  • 0 kudos

what are the PSPICE parameters to be defined to set alphaT voltage temperature coefficient correctly ? Thank you.

simulation over temperature range +25°C to +107°C of SM6T10A, PSPICE model downloaded from STMicro site, is far from real behaviour. At +25°C, VBR = 10.12V for IR = 1 mA, at +107°C, VBR = 244.8µV for the same current. With alphaT = 7.3 10e-4/°C (see ...

TStem by Associate
  • 880 Views
  • 0 replies
  • 0 kudos

UART Transmitting problem

Hello,I am using the stm8l151... mcu and I am trying to send different strings via Uart1 to HTerminal. I have three different strings to send. The first two strings are transmitted completely but when the third one is being sent, it is truncated and...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.