Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error while debugging stm8l discovery board

hai ,while debugging stm8l discovery board i got an error shown below.i found the similar issue described in many forums, and the solution was specified to install the st tollset but still it doesnt seem to work.How can i solve this issue?Please repl...

0690X000006CsJtQAK.jpg
Amal Babu by Associate III
  • 690 Views
  • 0 replies
  • 0 kudos

gdi-error [40606]:

My MCU is STM8AF6226,when I compile the code,The compiler reminded me gdi-error just like as "Wed Dec 19, 2018 08:17:00: Failed to set configuration with MCU name STM8AF6226: gdi-error [40606]: Configuration error: detected MCU different from the sel...

STM8L001J3 TIMER2 does not operate.

Hi.I have a problem using STM8L001J3.TIMER2 does not operate.​void main(void){ CLK->CKDIVR = 0x00; GPIO_Init(GPIOB, GPIO_Pin_3, GPIO_Mode_Out_PP_High_Fast);​ TIM2_DeInit(); TIM2->CR1 = 0x01; // Counter enabled TIM2->ARRH = 0x00; TIM2->ARRL = 0x9E; ...

STM6600CS25DM6F PWR_EN pull low problem

We use STM6600CS25DM6F in our application. The Li-on battery is also used in the circuit. When we dis-connected the USB cable, the battery voltage was dropped from 4.3V to 3.6V for 0.3ms. The system power consumption is around 0.3A. This suddent drop...

0690X000006Cr2mQAC.jpg 0690X000006Cr2hQAC.jpg 0690X000006Cr2cQAC.jpg
TTeng by Associate
  • 867 Views
  • 0 replies
  • 0 kudos

How can I program the EVAL-IPFC01V1?

Posted on February 20, 2018 at 13:48Yesterday I started to work with the EVAL-IPFC01V1.Can I program the STNRGPF01 with the ST-LINK/V2 through the SWIM connector J2?Or I must use the UART J3 with the adapter in the box? In this case what is the corr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.