Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PCB field value

In the example of the I2C frame, it is written that the PCB field is 0x02 or 0x03.The table "PCB field of the I-Block format" says that b0 and b3 may change, but it is not written what the meaning of these bits depends on.Maybe someone knows?

PPost by Associate II
  • 1614 Views
  • 0 replies
  • 0 kudos

STM8s003f3 with i2c LCD (PCF8574AT I2C Module)

Hello Every one ,I am trying to use I2c based LCD with stm8s003f3 controller. the write i2c address is 0x3f I am struck at a point ,the code is stopped in endless loop in below functionvoid PCF8574_write(unsigned char data_byte){  I2C_GenerateSTAR...

pverm.19 by Associate
  • 1077 Views
  • 0 replies
  • 0 kudos

Battery overheated issue

I have Asus zen max pro set which has wonderful battery backup which gives the best battery standby time but it gets overheated fast to using it for a long time. I have contacted https://www.uaetechnician.com/asus-laptop-battery-replacement.html but ...

PJame by Associate
  • 770 Views
  • 0 replies
  • 0 kudos

Saving setup of the "Option Byte"

Hi everyone,I have the usual file.s19. I can set the 'Option Byte' up using the opportune tab in 'Cosmic'. Now I need to share my file.s19, but I need to share it with option byte already set up.Is there any way to do that?thanks Antonio

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.