Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello!The Cosmic compiler supports "weak" functions to override them in the future?
Hello,I am interfacing a stm8s003k3 MCU with 12c LCD but it is not showing any thing on display.It is stuck on I2C-> SR! shift register which is showing 0 but it should be 1.The i2c addres is 0x3F i have already checked the LCD with ARDUINO board it ...
This is regarding Example project STM8S_StdPeriph_Examples.i'm using STVD, Cosmic Toolset to build the project. it builds successfully in Debug mode.when i change the mode to release mode, build fails with one of the error as below#error cpstm8 ..\.....
while building the project i'm getting below error, Kindly guide us to solve this issue,..----------- Project discover - STM8 Cosmic - Configuration Debug -------------Compiling ..\..\src\stm8s_it.c...cxstm8 -i..\..\..\..\..\mail_sent +mods0 +debug -...
Hello. I use STM8L052C6T6 and Power is 3.3v.GPIO PB0 use External interrupt.It can 3.3V External interrupt input.Question: Can 5V External interrupt input?
Is there any example to implementing Zero Crossing Detection on STM8S207 or similar MCU.
hello, to develop board using STM8S001, I am looking for a graphical or block programming tool.May you help me?Henry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.