Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error creating process for executable cxstm8

I'm using the Cosmic Software 4.4.9.0 in ST Visual Develop 4.3.12  I can't compile it.I try to install again but it showing same error.i tried to set root path correct like this C:\Program Files\COSMIC\FSE_compilers\CXSTM8.Can any one help me to solv...

tvenk by Associate II
  • 2156 Views
  • 1 replies
  • 0 kudos

Jump to code in RAM

In the documentation for switching to low power run mode it mentions that you need to jump to code in RAM before shutting down the FLASH.How do you specify that code should be placed in RAM?OK Update:This is for the STM8L151F3.I found link to a sugge...

TVan.11 by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

I2C setting is not working for FP-ATR-LORA1 package (GNSS + LoRa asset tracker)

To reproduceEnable I2C in gnss_app_cfg.h#define configUSE_I2C 1When moved, the UART log said(11:58:08.056) -->�?�Going�?�to�?�run...(11:58:12.943) Can�?�not�?�read�?�axes(11:58:12.963) >>�?�sensor_event(11:58:15.875) Accelerometer�?�NOT�?�initialized...

SVora.4 by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

VN380SP

I can't find any information about VN380SP at the st.com siteIs VN380SP discontinued? Deprecated product?

AShab.10 by Associate
  • 699 Views
  • 0 replies
  • 0 kudos

STM8: mistake in datasheet?

Good morning.STM8S003: https://www.st.com/resource/en/datasheet/DM00024550.pdfOn a page 45 under table 15 (quote):"2. Do not use more than one remapping option in the same port. It is forbidden to enable both AFR1 and AFR0."Here first part of the sen...

Arlleex1 by Associate III
  • 821 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.