2019-02-04 9:01 PM
To reproduce
#define configUSE_I2C 1(11:58:08.056) -->�?�Going�?�to�?�run...
(11:58:12.943) Can�?�not�?�read�?�axes
(11:58:12.963) >>�?�sensor_event
(11:58:15.875) Accelerometer�?�NOT�?�initialized
Everything is ok for default UART setting. One possible issue is the configuration of I2C1 in interrupt mode for Teseo component with background reading.
2019-03-13 6:03 AM
Hi
In the FP-ATR-LORA1 the GNSS is not supported on I2C bus.
It's a design decision because GNSS (in Geofencing mode) is used to wakeup the whole system (from standby) sending a message via UART.
This can not be done on I2C.
Hope this helps
Regards
Francesco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.