Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi, I use CLT01-38SQ7. In datasheet (DocID028182 Rev 1) is not clear to me how to use Vcs pin (24V sensor power supply sensing input) for UVA purpose.In Figure 7. “Logic status of the SCLT3-8BQ7 power supply�? voltage ranges of Vcc and Vc are shown, ...
We are using USBUF01W6 as EMI filter for STM32F207VCT6 in USB D+ and D- lines in Full speed mode and we have connected VBUS (5V) at pin 3.3V pin of USBUF01W6. Does this make sense to you?NOTE: This question and answer originated from a customer suppo...
I have to read this ARM926 by JTAG connections but I don't have MCU pinout. On web I can only find a datasheet without pinout description.
Hello...Is the STG3157 suitable for headphone-level audio? I need to switch between the inputs of two microphones and put one of them into a small audio amp IC.Thanks!--Jim Newton
Hi, I have searched and could not find any information about the Accordo5 nor Accordo2 SOC in the entire community. Even the Accordo5 product page do not contain much information. I am at loss to where to get information about the complete tool chain...
When we debug with ST-link/V3set on STVD, we found this issue swim prog error[42007] buffer program error.but we didn't found this issue with ST-link/V2.How does solve this issue when we used the ST-link/V3set ?
How for example do I initialize all 3 devices, where addressing and necessary parameters are concerned. Any sample code or advice in this regard would be very welcome. (RTC : either PCF8563 or DS1307; I2C LCD with PCF8574 expander and 24c32 or 24c64...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.