2019-03-27 7:48 AM
We are using USBUF01W6 as EMI filter for STM32F207VCT6 in USB D+ and D- lines in Full speed mode and we have connected VBUS (5V) at pin 3.3V pin of USBUF01W6.
Does this make sense to you?
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.
Solved! Go to Solution.
2019-03-27 7:50 AM
As STM32 used already includes series resistors for USB D+ and D-, the right part to protect against ESD on D+ and D- is USBLC6-2SC6, instead of USBUF.
In addition, you should consider to protect 5V_USB against ESD and EOS transients (8/20µs). We recommend to use ESDA7P60-1U1M or ESDA7P120-1U1M. In this case, VBUS of USBLC6-2SC6 is connected to a 100nF capacitor or left open.
For best protection these parts should be placed as close as possible to the connector.
2019-03-27 7:50 AM
As STM32 used already includes series resistors for USB D+ and D-, the right part to protect against ESD on D+ and D- is USBLC6-2SC6, instead of USBUF.
In addition, you should consider to protect 5V_USB against ESD and EOS transients (8/20µs). We recommend to use ESDA7P60-1U1M or ESDA7P120-1U1M. In this case, VBUS of USBLC6-2SC6 is connected to a 100nF capacitor or left open.
For best protection these parts should be placed as close as possible to the connector.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.