Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Init() bug for more than one UART setting

I am working on a LoRaWAN and GNSS project. I have found one inconsistent operation when try to configure UART1 for GNSS connection. UART2 is used as PRINTF for logging.   Procedure to produce bug: Use I-CUBE-LRWAN example as the codebase.Add code fr...

SVora.4 by Associate
  • 2350 Views
  • 3 replies
  • 1 kudos

Invalid SPICE model IGBT STGW20NC60VD.

Hi.Now I am composing the model of the device in the program Microcap using SPICE model of IGBT STGW20NC60VD. This transistor has current-voltage characteristics shown Figure 1. But SPICE model of transistor has other different characteristics (Fig. ...

AVoro.10 by Associate
  • 1317 Views
  • 0 replies
  • 0 kudos

STM8L1528 ADC, DMA, TImer not working together.

Hi there,I am developing code for STM8L1528 EVAL board. My goal is to configure adc with dma(peripheral to memory) where adc should collect data for certain period, for example, 2 seconds.So I configured adc and dma according to examples codes given....

Gopal by Associate
  • 1148 Views
  • 2 replies
  • 0 kudos

External Interrupt in PORTB (Multiple pin)

I configure the portB 4,5,6,7 as external interrupt pins. the program is working well if any interrupt occurs in portb 4,5,6,7 the execution send to irq. how to find which pin irq is occured in portbplease give the solution to my problem

RKuma.7 by Associate
  • 946 Views
  • 2 replies
  • 0 kudos

Timing calculation of Adc intterupt

Hello sirI am use stm8s​ for measuring voltage rms​So i use adc but how to calculate when adc interrupt are coming​I Aattched initiation code in this post​​i try to calculate adc interrupt time but when i measure it is wrong​Plz provide guidance how ...

Hiren by Associate III
  • 1578 Views
  • 1 replies
  • 0 kudos

How to know which is the pin #1 of a M95M02-A125?

The M95M02-A125 has SO8 package. I can't see any mark or anything that shows which the pin number 1 is. I may suppose it's according to text orientation, but it's just a guess. So, the question is: how to know the right orientation of the chip?Thanks...

JPied by Associate
  • 2751 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.