2018-10-14 1:44 PM
Hello.
I'm trying to set Option bytes on STM8s005k6 from main code, but still I'm getting error in complementary bytes (when I try to rad out it back in STVP) and MCU hangs.
I'm using SDCC compiler with this code:
// Set option bytes because of buzzer
if(OPT->OPT2 != 0x80 || OPT->OPT3 != 0x08){
FLASH->CR2 |= FLASH_CR2_OPT; //unlock option bytes for writing
FLASH->NCR2 &= (uint8_t)(~FLASH_NCR2_NOPT);
while (!(FLASH->IAPSR & FLASH_IAPSR_DUL));
OPT->OPT2 = 0x80; // enable LSI clock source
OPT->NOPT2 = 0x7f;
OPT->OPT3 = 0x08; // set PD4 as alternative buzzer output
OPT->NOPT3 = 0xf7;
while (!(FLASH->IAPSR & FLASH_IAPSR_EOP)); // wait for write finish
FLASH->CR2 &= (uint8_t)(~FLASH_CR2_OPT); //lock back
FLASH->NCR2 |= FLASH_NCR2_NOPT;
}If I set it through graphic STVP and read OPT2 and OPT3 registers, they have exactly these values. But from code it doesn't accept :\
Thank you for any tips.
2019-07-01 5:25 AM
2019-07-07 9:34 AM
Hello Daniel!
Ofcourse the MCU hangs. On line 5, in the while loop you wait for the DUL flag to be set, but you never write the unlocking keys to DUKR register.
You need to write the 2 hardware keys in FLASH_DUKR register, than you can check if DUL flag is set - please check the Reference Manual for more details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.