2019-08-22 7:09 PM
static void TIM1_Config(void)
{
CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);
TIM1_DeInit();
// 2m/ 40
TIM1_TimeBaseInit(39, TIM1_CounterMode_Down, 0xffff, 0); //timer freq = (clock CPU/16) -> 1bit = 1uS -> 92*1uS=92uS
TIM1->EGR |= (1 << TIM1_EGR_UG);
//TIM1_CCPreloadControl(ENABLE);
//TIM1_ITConfig(TIM1_IT_Update, ENABLE);
//TIM1_Cmd(ENABLE);
}does the code generate some speed interrupts ? it makes code run error
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.