Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to reduce the power consumption of STM8S001J3M3TR mcu in order to meet standby mode < 0.5W requirement.

Hi All,STM8S001J3M3TR is used in our product. From the spec of this MCU, it said that it only consume around 4mA in running mode. So, I chose this IC in our project. After I get this IC and check it. When no IO operation is performed, this MCU consum...

NKa L by Associate
  • 1426 Views
  • 2 replies
  • 0 kudos

I need to program the ST8L101F3P6 with ST viual

hi,       I am using ST8l101F3P6 microcontroller.I have used ST Visual develop with Cosmic compiler.I Programmed and compiled successfully.but I can not Program the controller with ST visual programmer..when I try to program it asks to check the conn...

karthik.b by Associate II
  • 2755 Views
  • 4 replies
  • 0 kudos

stm8s_adc1 SPL files throwing compiler errors

Further to my previous message I have setup a new STVD workspace, included stm8s.h and just stm8s_adc1.c and .h, setup processor etc and get 150+ compiler errors on stm82_adc1.c just as if the header file was not specified but it is. So having reduce...

BCowa by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos

Why I fill wrong TIM2 registers when I run STM8S103 with en.stsw-stm8069 (I see in debug mode) TIM2. IDE=IAR ??

Hello everyone, I am running STM8S103F3P with IAR. I downloaded this: en.stsw-stm8069.In IAR chosed my micro STM8S103F3P. But as I see in debug mode I fill wrong register (TIM2) at init TIM2 regs. It seems setup (config) in IAR is wrong or I did som...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.