Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD LD mem,A problem

In STVD (ver.4.3.12 MCU: STM8L052C6)I wrote:LD A,#$68LD $5232,A   ;(USART bade rate register)but memory ($5232) is $00when I wrote: LD $5000,A ;Port A data reg. memory ($5000) is $68, it work wellwhai is the different?Could anybody hel...

Has the EEPROM M95256-W an ECC?

The old M95256-W datasheet Rev. 6 says:"The M95256-W and the M95256-R devices (2.5V and 1.8V versions, processed in F8 andidentified with the letter "A") offer an ECC (Error Correction Code) logic"The new version Rev. 21 says:"M95256 and M95256-D dev...

Manfred1 by Associate
  • 914 Views
  • 1 replies
  • 0 kudos

I need PSD301 Programmer

Does anyone know where I might be able to find PSDPRO programmer and WS6102 socket? I need to program an PSD301.I have UV windowed PSD301 it erased well.tried with my 3rd party universal programmer but failed to wrote.somebody help me..Thanks.

is the i2c init function right?

void sEE_Init(void) { //printf("i2c init\n"); sEE_LowLevel_Init(); // enable clock   /*!< I2C configuration */ /* sEE_I2C Peripheral Enable */ I2C_Cmd(sEE_I2C, ENABLE); I2C_DeInit(sEE_I2C); /* sEE_I2C configuration after enablin...

Hello, I hope i am posting this to the correct area.. I am looking for some help/guidence implementing the VNN1NV04 3-terminal protected MOSFET.

The application is a solenoid driver, 12V 0.5A running PWM 1Khz. It's a very basic low side application, diode across the coil. The signal is 5V logic from a microcontroller.I have read the datasheet, and the application note AN4798. to be honest som...

Spwf04s could not turn on radio afer reset? The module work ok before. Now the radio could turn on after power on . Then initiate and reset wifi module.The radio could not work . why?

[17:13:18.309]ÊÕ¡û¡ô+WIND:1:Poweron:171117-0328fe3-SPWF04S+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SC+WIND:65:Factory Reset:1+WIND:0:Console active+WIND:3:Watchdog Running:20[17:13:19.307]ÊÕ¡û¡ô+WIND:32:WiFi...

Wsl by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.