Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Strange tim4 interrupts?

The chip is stm8s103f3p6, and I wanna use lsi as clk and tim4 to make a timer, there are two strange things happened.​ when I set prescaler to TIM4_PRESCALER_4 and ARR to 32, I thought it should interrupt every 1ms (128k/4/32=1kHz), but it seems brea...

hpare by Associate
  • 1024 Views
  • 1 replies
  • 0 kudos

Interrupt vector relocation in stm8

Hi,​I​ am developing an IAP for one of my project.In that the bootloader and the application using interrupt vectors.How can I seperate the ​interrupt vectors for application as well as bootloader. How to relocate the interrupt vectors in STM8?​T...

leojo by Associate
  • 1196 Views
  • 1 replies
  • 0 kudos

Resolved! STM8L001J3 : SWIM and reset pin

Hello,I would like to use the STM8L001J3. I am very new with STM8 family. I used to using STM32. STM8L001J3 seems to be great for my application, i started to draw the schematics but i wonder how to connect the debug probe. For VCC, VSS, and SWIM pin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.