Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 24C256 EEPROM Page Write

Hi there ! I hope someone can help me with a confusion i had in my mind right now. I work with a EEPROM 24C256 and need a write a lot of data inside , soo i decide to use the page write solution . So from the datasheet i saw i can write 64byte in one...

Immagine 2025-09-15 152315.png
SGian.1 by Senior
  • 7032 Views
  • 3 replies
  • 2 kudos

GT9271 TOUCH INT

Hi there. I require assistance to ensure the proper operation of GT9271.After properly RESETting the GT9271, and issuing the 0XBA I2C address, the device keeps pulling the INT pin without any touch on the LCD display (1024x600). I really feel a lack ...

Sem título.png
m-a-c-f by Associate III
  • 5898 Views
  • 13 replies
  • 5 kudos

Resolved! About the operation of the STG3157

”Switch S1 is ON (connected to common port D) when the IN input is held high, andOFF (a high impedance state exists between the two ports) when IN is held low.Switch S2 is ON (connected to common port D) when the IN input is held low andOFF (a high i...

Resolved! Blue and Black Pill SWO debugging

Split from STM32H5 SWO debugging.I want use SWO pin like standalone debug. Send data by "ITM_SendChar('A');" and want to read data from SWO pin by USB-UART dongle, SWO pin => Rx pin UART-USB on PC.I try blue and black pill (STM32F103 and STM32F411), ...

mkigor by Associate II
  • 1844 Views
  • 13 replies
  • 7 kudos

Hysteresis module for STSW‑TTPPFC01

Hello, I am conducting research on the design of a single-phase PFC in totem-pole topology. In this context, I am studying the STEVAL-TTPPFC01 prototype and the STSW-TTPPFC01 firmware. I used the eDesignSuite tool to generate the code under STM32Cube...

Flbou by Associate
  • 1252 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.