Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

logarithm calculation problem

i need to calculate some log based contents using ST visual develop IDE and Cosmic compiler. but "log" is not recognized by compiler. any solution pleaseexample: my_reg=log(reg1);regards.

Nyous.1 by Associate II
  • 903 Views
  • 1 replies
  • 0 kudos

ATM8AF: activate Ports for GPIO usage

Hello Community,I'm struggeling with the GPIO activation of Pin PB0.My Setup is: µC: STM8AF6213PCA with TSSOP20 Pinout, STVD + Cosmic C CompilerIt is no problem to aktivate the Port C (PC4, PC5, PC6 and PC7). But port B seems to be dead.But the port ...

0693W000004IFIvQAO.png
SWiel.1 by Associate II
  • 843 Views
  • 0 replies
  • 0 kudos

CANBus, Ethrnet and RS232 on the same MCU

Hello for a project I will be using Ethernet, CANBus and RS232. Now the maximum frequency for CANBUS is 1 Mbit per seconds, for RS-232 that is 20 k baud and for Ethernet I think it is again 1 Mbit per seconds. So with a MCU that has at least 2 MHz c...

GunkutA by Senior
  • 1757 Views
  • 3 replies
  • 0 kudos

UART issue for reading 2 or more bytes length

I am having an issue with the UART1 communication between two devices (Computer and a STM8S208 board).I implemented software in the computer that writes two bytes length of data to the STM8• the first byte that acts as an identifier;•the second byte ...

0693W000004GyvoQAC.png
GGhed.1 by Associate II
  • 3257 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.