2020-09-25 9:56 PM
I'm using Comparator 2 on the STM8L151G4 with DAC1 on the inverting input. When the DAC outputs 0V, the current draw during Halt mode is < 1 uA. If the DAC outputs around 0.5V before the program enters Halt mode, the current draw is 80 uA in Halt mode. Is there any way the DAC output voltage can be maintained during Halt mode and draw less current?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.