Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to compile code in STVD

when I compile the code for a simple GPIO toggle, it shows an error like thisCan't understand what is the issue, I have included all the inc and source files into the project from the Standard peripheral library and the Cosmic compiler is also succes...

0693W000006H8G5QAK.png
KGupt.1 by Associate III
  • 875 Views
  • 2 replies
  • 0 kudos

STM8 project compile failed

Hi, i try to compile the example which get it from the library using STVD, but it failed. the attachment is the whole work space. can please help check where is the wrong setting.

ALiu.5 by Associate II
  • 603 Views
  • 0 replies
  • 0 kudos

STM8S power (current) consumtion problem

I'm developing some applications with STM8S003K3 now (battery-used product). The problem is that, I cannot make the MCU consume just 4.5 micro-ampere order current in the halt mode as in the datasheet described.I use the Eval-Board "STM8SVLDISCOVERY"...

MBern.5 by Associate
  • 1536 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.