Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SRC0CS25D !!!! In the material of the SRC0CS25D, there is threshold voltage and what is for in this component?

I did not understand that VCC range of the SRC0CS25D is 1V6-5V5 and the electrical specifications state Vth=(min,type,max)=(3v29,3v40,3v50). There is some uncertinity about the thereshold. If my VIN voltage (given to VCC pin of SRC0CS25D) is under 3....

Why RTC_WakeUpCmd can fail?

In the STM8L SDK, the RTC_WakeUpCmd()  function can return an ERROR if the WUTWF bit fails to be set after a delay.  In the RM there's no mention of how and why this situation would occur.Why RTC_WakeUpCmd can fail?Thanks,Gabriel

0693W00000AMn9zQAD.png 0693W00000AMn8SQAT.png
GBert.2 by Senior
  • 1389 Views
  • 0 replies
  • 0 kudos

stm8l151g4 DMA USART recieve only once

Hi.i'm try using USART1 and recieve bytes with DMA from SBUS transmitter.. But have strange problem - i'm recive only once and later DMA IRQ TC2 never occure. I'm try many variants - all not help me(((Here my some code - #define USART_DMA_CHANNEL_RX ...

Esten.11 by Associate
  • 1460 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.