Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi there! I wanted to politely ask for your help, if you can answer a simple question: i have a 950406 k128 eeprom chip but cant find one to buy online i only can find 950406 K506W or 950406 K304K, if so can i use these other ones to replace the950406k128

It is for a veglia boreti automotive instrument cluster from a fiat punto 2001 - 1999Hi there! I wanted to politely ask for your help, if you can answer a simple question: i have a 950406 k128 eeprom chip but cant find one to buy online i only can fi...

0693W000008zx6MQAQ.jpg
NKiri.3 by Associate II
  • 2234 Views
  • 4 replies
  • 0 kudos

The problem is that the controller of stm8 doesn't work after it has been used on the vehicle for a period of time, and the controller function is invalid. Once in the past, the controller can work normally after re burning the program, but this time ther

The problem is that the controller of stm8S208C8T6 doesn't work after it has been used on the vehicle for a period of time, and the controller function is invalid. Once in the past, the controller can work normally after re burning the program, but...

Wzhan.5 by Associate
  • 1257 Views
  • 1 replies
  • 0 kudos

STM8AL3189 flashing of image on address above 0xFFFF that code is not working and using STVD tried

Hi Team,I am using the STM8AL3189 controller, created 2 images where,1st image will flash with 0x8100 to 0xffff and 2nd flashing of the image will flash on 0x10000 to 0x17fff (address above 0xFFFF )we have changed the linker file with the startup fil...

0693W00000AMQ3oQAH.png

STM8L050J3 SON8N - how to generate PWM on PC5 ?

Hello,I am trying to generate a PWM signal on pin PC5 using TIM2_CH1 , but no success. But I am able to generate PWM on pin PD0 using TIM3_CH2.Normally the procedure is quite simple :for TIM2_CH1 - pin PC5 TIM2_OC1Init(TIM2_OCMode_PWM1,  TIM2_OutputS...

0690X000009Yx7yQAC.png 0690X000009Yx7jQAC.png
SDomn by Associate
  • 1478 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.