Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S007C8T6

Hi ST team, We bought 4500pcs STM8S007C8T6, COO is Malaysia, but MSL on the label is MSL 2, is it correct? Because we found official datasheet for this P/N is MSL 3. Could you please help explain why one P/N with two MSL? Thank you.

LWU.31 by Associate II
  • 835 Views
  • 0 replies
  • 0 kudos

Request product confirmation

HiThe product in the picture we attached is damaged and is about to be replaced.It is difficult to find information about the products below.Can I get the same product?Also, is this an EEPROM?Answers I'll wait.thank you.

YPark.6 by Associate
  • 1792 Views
  • 3 replies
  • 0 kudos

Resolved! AS21P2TLR peak switching energy

I have a capacity of 40nF on the S2 pin, charged to a voltage of 3.3V.The D pin is at GND. The 40nF is then discharged through the analog switch. The peak current will be around 6.6A for a very short time (if the analog switch has 0.5 Ohm resistance)...

MSchi.3 by Associate
  • 1264 Views
  • 1 replies
  • 1 kudos

#error cpstm8 main.c:1(0+7) missing ;

include "stm8s.h"             #ifdef USE_FULL_ASSERT   /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: a...

MKUMA.31 by Associate
  • 2197 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.