I need an Account Manager or ST Micro Sales Rep for Broadcom project
Please check who is Broadcom Account Manager in ST Micro, and please reach me at:sean-sc.chen@broadcom.com
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Please check who is Broadcom Account Manager in ST Micro, and please reach me at:sean-sc.chen@broadcom.com
Hi,Can USBLC6-4SC6 be used to protect an IO from EFT (IEC 61000-4-4) and lightning (IEC 61000-4-5)? I do not see any specification for these standards? Thanks.RegardsGordon
I am working with the M95M04-DR eeprom. In my program, I must save logs of data inside the EEPROM memory. I wriite data in chunks of 25 bytes.I have written 11 chunks of data ant noticed a problem. I have a function to read back multiple bytes of dat...
How can I fix the super long delay and weird ACK glitch with I2C on STM8S?I'm having some troubles with I2C communications between a raspberry pi and STM8S. The STM8S is a slave transmitter and I2C is running at 100 KHz. It works much the time, but I...
I am writing from an esp32 I2C master to a stm8s103f mcu. My scope shows the esp is sending a clean read addr byte onto the scl/sda pins (PB4/PB5). But the stm8 is not running my interrupt routine. I have a gpio pin that should toggle when the interr...
Reading the data sheet of SMCJxxA, SMCJxxCA,for the SMCJ5.0A/CA it is specified an IRM of 500uA ( 2000uA at 85C) at 5V it seem not consistant whith the SMBJ type witch seem to be the same (exept power handling).(In SMBJXXA data sheet miss witch is bi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.