Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
At the moment I have ST MV C737, how I understand it is zener diode, but no info in internet and here. Anyone can help to identify?
Hello ST,I’m attempting to integrate the STEVAL-STRKT01 into my system.I need to issue NMEA commands to the Teseo .I’m connected into the UART over CN503 (TX,RX,GND only) and I can see the serial chatter.For example, I want to Stop the STAGPS engine ...
We cannot find any info about the \K and /HFWhen we try to use the /HF, which looks like it is polarized, but in TMMDB3 datasheet, it never mentioned. So we want to clarify.
Hello,I am an auto parts developer.I am using the M24512-A125 product.I am writing 1 page of address 128 bytes.I am writing the same data by 3 bytes.I am writing 42 bytes of different data.I am writing 42 bytes * 3 bytes = 128 bytes.I am using Nbytes...
Dear sir/madam,where is the right place to program stnrgpf01 online by edesignsuite? I logged into eDesignSuite but didnt see the choice of stnrgpf01.Thanks,Michael
ONSEMI MPNNC7WZ16P6X NL27WZ16DFT2G NC7SZ74K8X NL17SZ74USG NLV17SZ74USGNC7SZ125P5X NL17SZ125DFT2GNC7SZ74K8XNC7SZ27P6X, SN74LVC1G27DCKR
I've been using vscode as my editor since the one in stvd seems to have features from 15 years ago. I have files also open in stvd since clicking on errors opens files. This means that when I switch to stvd from vscode I get the warning about files...
In our application USBLC6-2P6 is connected between a USB port and a processor STM32L4R5xx. The circuit is self-powered (Li-ion battery), and uses either PC USB or USB dc power supply for charging and communication. We find a number of damaged USBLC...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.