Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Blue pill Freertos

Hi,I am planning to use STM32 bluepill board with Freertos. Hence trying to use Freertos API. I wanted to know how the CUBE IDE makes sure that API call to Freertos doesn't transform into an API call to Linux OS on which CUBE IDE is installed during ...

bdpak by Associate II
  • 4944 Views
  • 6 replies
  • 2 kudos

Triac BTA41600B

hey guys,I need to buy a new Triac, the old component is BTA41600B, but there are other letters after this specification, for example: BTA41600B 7SABK VU PHL 7S 135.I would like to know about this feature 7SABK VU PHL 7S 135, as these BTA41600B I fou...

mendonca by Associate
  • 2247 Views
  • 2 replies
  • 1 kudos

IBIS MODEL

Hi Team, We are looking IBIS model for the ITA25B1RL.To simulate SI, required IBIS model. Please provide.Thank you 

Damo by Associate
  • 1132 Views
  • 0 replies
  • 0 kudos

Resolved! Marking STM8L151F3U6TR

Hi, I have bought the parts STM8L151F3U6TR. The marking indicated in datasheet is L526. However, marking on component is L536. Anyone can confirm this marking of L536 is correct? 

Resolved! M24512-W

Hi,I need help to identify a 512 Kbit serial I²C bus EEPROM from the M24512 series.I have two differents parts which appear identical, apart from one letter at the end of the reference : M24512-WG for the first one and M24512-WP for the second (photo...

pepito60 by Associate II
  • 10916 Views
  • 12 replies
  • 8 kudos

eDsim

Hello, i would like to simulate a schematic of a 100W USB PD adapter that include the STUSB4761 usb pd controller using eDsim but i can’t find the controller in the library can any one help me please.

nesrine12 by Associate III
  • 6395 Views
  • 1 replies
  • 0 kudos

L6470

Hi,I am usinga) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.b) I am using 24VDC for L6470.c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase. ...

CSu.12 by Associate II
  • 1505 Views
  • 0 replies
  • 0 kudos

Spice Model required for VIPERGAN50TR

Hi,Greetings,I have been using VIPERGAN50TR part quite some time. Now I want run simulation regarding the same.Kindly help me in finding unencrypted spice model.Thanks and Regards,Utham

UV by Associate
  • 1439 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.