Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot access >=3,3V at GPIOA - STM32F411

Dear Ladies and Gentlemen,   for you it is your daily business - for me as customer a contemporary challenge:   Something went wrong with my pin-configuration. I measure ~1,7 V as GPIO-output of Port A instead of wished >=3.3 V. My power supply is a ...

timbo2023 by Associate III
  • 33248 Views
  • 46 replies
  • 20 kudos

Resolved! Triac ASC 108 6S FQ41

Bonjour,J’ai un composant qui est détruit sur une carte mère, l’ancienne référence ST est ASC 108 6S FQ41.Pouvez-vous me donner la nouvelle référence qui correspond à ce triac.Je vous remercieBonne journée

Duval by Associate
  • 2172 Views
  • 4 replies
  • 0 kudos

Unknown TSSOP-20 chip identification

Hi all.I'm struggling with certain device and I'd like to identify unknown TSSOP-20 chip on the PCB. Chip must be an MCU and based on the pinout it's very close to some STM8, eg. STM8AF6213. There are VCC and GND connected to Pin 9 and 7 respectively...

MPrih.1 by Associate
  • 4324 Views
  • 4 replies
  • 0 kudos

STHV1600 custom waveform generation

Hi all,I have been testing the STHV1600 evaluation module and want to generate a continuous wave (CW) that would change after some time. Currently, the STSW-IME014 GUI software seems to allow creating multiple CW patterns and assigning them to a spec...

Bartas by Associate
  • 1000 Views
  • 0 replies
  • 0 kudos

Configuration of STHV1600

Hello, folks.I'm using the STHV1600 (specifically its evaluation kit board, the STEVAL-IME014V1B) for my thesis on sonothrombolysis. For this ultrasound application, I need multiple time delay configurations for the pulses (approximately 400). The GU...

RHRPMICL1AK01V

Dear, I'm trying to find pricing +  a European distributor that are able to deliverRHRPMICL1AK01V Can anybody help? For the moment, I got no helpful feedback from usual distrubutors Thanks, Nicolas.

IWDG STM8

Hello,STM8S208RB microcontroller, Independent watchdog (IWDG). After starting the watchdog timer (command KEY_ENABLE value = 0xCC), I understand that the watchdog timer stops after resetting the microcontroller. The default register state is undefine...

MykolaLevun_0-1707560153755.png

M95040 Registers definition

Hi,We are using M95040-DFMN6TP SPI PROM on our board.The Serial Input/ Output timing given in the datasheet is not detailed.There is not much info on the address width and data width, and how to control write/read, there also isn't the register defin...

Ravikumar by Associate II
  • 2296 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.