2004-04-26 6:08 PM
Asking about Auto Reload Timer interrupt in ST7FLITE29
2004-04-25 11:16 PM
Hi! there!
I would like to ask about using ART of ST7LITE. I am using ST7FLITE29 in my project. As I know that ART is 12bit free-running upcounter. I am using an ART with 1ms timebase clock. and I have set the value of ATR to (4096-20). (it will make ART interrupt every 20ms) my question is Do I need to wait for 4096ms, until first overflow interrupt occur?? I want to start counting(every 20ms) as soon as power-up. give me some advice! have a nice day !!2004-04-26 6:08 PM
The counter is incremented continuously as soon as a counter clock is
selected. First time it starts from 0. When a counter overflow occurs, the counter restarts from the value specified in the ATR register.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.