2007-01-15 10:11 PM
2007-01-04 9:41 PM
Hello Folks,
i programmed the ART as freerunning Timer. Fosc= 3,6864 MHz, ClkDiv= 3, Prescl= 128 Fin= 9600, RC= 10h If my Calculations are correct, the above Settings = 25ms. The Overflow Interrupt is used to update some Calcs(Tcyc.As far as i know, ARTs need no additional cycles for INT and Reload. They run and run until RESET. OK, the INTMASK must be written but it have no effect on the running Timer. Hey, its Hardware. Is it the same with the ST6265 ART. Or are there add. Cycles? best regards Andreas2007-01-15 10:11 PM
Hi again,
there are ''dead'' cycles when using the ART as INT source. To check this out, i programmed a simple software RTC using the ART OverflowINT as Timebase. Every INT increments a register til 40d. 25ms*40=1s. result: the clock runs ahead. question: WHY? AndreasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.