2007-05-06 10:07 AM
Annoying error when programming a STR911 with IAR for the 2nd time.
2011-05-17 12:42 AM
Hello,
I just got a new annoying error when I try to debug a STR911FM44X6 processor with IAR’s ide for the second time. After I execute an Erase operation with the JTAG programmer, I can download and debug the program, with no errors at all. But, when I attemp to do it a second time, I get this error message: “Write memory error @ address 0x04001400, word access: Memory access timeout.� So, I have to unplug the J-Link programming cable, attach it to a FlashLink JTAG programmer that I made, execute an Erase operation, and now I can download the program again… quiet annoying. Is it a problem with “91x_caps.c� definitions? Or maybe a “91x_conf.h� declaration ? Thank you for your help. Mark2011-05-17 12:42 AM
Hi Zouhair,
I downloaded the newest drivers from IAR (http://supp.iar.com/FilesPublic/SUPPORT/002811/JLink_3.68B.zip) and followed all the instruction within the readme file, but with no success. The error message keeps poping up. I've selected both options to reset the proceesor by hardware in J-Link/Setup. And I've created 3 different workspaces/projects just to be sure I wasn't missing any detail. The only reason I moved to ARMs was because a needed a faster processor, but after losing so much time trying to solve IAR's ide problems and mysteries, I really miss my Microchip's MPLAB. Mark2011-05-17 12:42 AM
Hi Zouhair,
I did a fresh install in another computer. Now, I only has to use the JTAG programmer once every 5~6 programming cycles to erase the ARM, when the error pops up, which is ok with me. When I use the STR912-SK everything is fine, but when I use the STR911... things get rough. Is there anything different in the configuration files between these two processors, besides the missing GPIO0,1,7,8,9 ??? Mark.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.