2014-05-06 5:56 PM
I'm using the STM8L101F3 with IAR. I would like to set and clear the Activation level bit.
There is no library function to access this and I'm not sure how to access this register from code. Looking at iostm8l101f3.h, the register and bit is defined: /* Global configuration register */ #ifdef __IAR_SYSTEMS_ICC__ typedef struct { unsigned char SWD : 1; unsigned char AL : 1; } __BITS_CPU_CFG_GCR; #endif __IO_REG8_BIT(CPU_CFG_GCR, 0x7F60, __READ_WRITE, __BITS_CPU_CFG_GCR); #define CPU_CFG_GCR_AL CPU_CFG_GCR_bit.AL But trying to modify the bit from code using: CPU_CFG_GCR_AL = 1; generates an error: Error[Pe020]: identifier ''CPU_CFG_GCR_AL'' is undefined How can I modify this bit?2014-05-07 4:12 AM
Ok, resolved it:
CFG->GCR |= CFG_GCR_AL;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.