2021-09-22 10:04 AM
I am a starter for stm8 mcus
I installed STVD and COSMİC C Compiler.
at first step
-i can not save my project
-i can not uncomment my mcu in stm8s.h header file
I get an error message
"Access to C:Users\R&P\Desktop\first\inc\stms.h"
Access to C:Users\R&P\Desktop\first is my folder created for workspace.
SPL files are in folders named inc and scr . these two folders are inside the project folder.
everything looks very simple but there is a problem.
Can it be because of & in file path definition?
Access to C:Users\R&P\Desktop\first\
2021-09-22 11:26 AM
Are the files Read Only? Check attributes
Yes, I would avoid spaces and special characters in file names and paths. Applications may be less tolerant than the OS
Also I'd generally avoid using the Desktop for files/directories.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.