2022-04-22 10:01 AM
1. What happens if TIM2_ARR is 0xFFFF? Does overflow occur when timer counter counts past 0xFFFF?
2. What happens to compare output after TIM2 overflows? For example, lets say that the TIM2_CCR1 = 0x7FFF so the output changes state when the counter counts past this value. So what happens to the output when the counter counts past 0xFFFF?
Solved! Go to Solution.
2022-04-22 1:56 PM
I'm not working on STM8, but many peripherals are almost the same and the reference manual seems to confirm that.
RM0016 section 17.3.4 doesn't differentiate 0xFFFF from other values:
In up-counting mode, the counter counts from 0 to a user-defined compare value (content of the TIM1_ARR register). It then restarts from 0 and generates a counter overflow event and a UEV if the UDIS bit is 0 in the TIM1_CR1 register.
Probably you should change the way you think about it. You think that it overflows, but actually it never counts past 0xFFFF. Instead it generates an update event the same way as with other ARR values.
2022-04-22 1:56 PM
I'm not working on STM8, but many peripherals are almost the same and the reference manual seems to confirm that.
RM0016 section 17.3.4 doesn't differentiate 0xFFFF from other values:
In up-counting mode, the counter counts from 0 to a user-defined compare value (content of the TIM1_ARR register). It then restarts from 0 and generates a counter overflow event and a UEV if the UDIS bit is 0 in the TIM1_CR1 register.
Probably you should change the way you think about it. You think that it overflows, but actually it never counts past 0xFFFF. Instead it generates an update event the same way as with other ARR values.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.