cancel
Showing results for 
Search instead for 
Did you mean: 

Would you recommend any additional specific SW I could use for Decision Trees generation or specifically with SensorTile.box?

Evelina CAMILLERI
ST Employee

 [webinar - Program decision trees in sensors with a Machine Learning Core]

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Evelina CAMILLERI
ST Employee

Yes, we suggest to adopt Unico GUI because all the MLC process is easy with just one tooI, but you can approach the Machine Learning process in other ways.

For example, the decision tree can be built also using external tools such as Weka, Python, RapidMiner and MATLAB. The output of these external tool is always compatible with Unico (for Python and MATLAB we provide some script as examples in our GitHub repository: https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/tools).

All these external tools are also described in the appendix sections of the MLC application notes of our devices. 

Using the SensorTile.box, in the first step of the MLC process, data can be captured through the "ST BLE Sensor" app and stored into the SD card. Then data logs can be dowloaded on the PC, and the MLC configuration process can be implemented using Unico GUI.

View solution in original post

1 REPLY 1
Evelina CAMILLERI
ST Employee

Yes, we suggest to adopt Unico GUI because all the MLC process is easy with just one tooI, but you can approach the Machine Learning process in other ways.

For example, the decision tree can be built also using external tools such as Weka, Python, RapidMiner and MATLAB. The output of these external tool is always compatible with Unico (for Python and MATLAB we provide some script as examples in our GitHub repository: https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/tools).

All these external tools are also described in the appendix sections of the MLC application notes of our devices. 

Using the SensorTile.box, in the first step of the MLC process, data can be captured through the "ST BLE Sensor" app and stored into the SD card. Then data logs can be dowloaded on the PC, and the MLC configuration process can be implemented using Unico GUI.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.