2020-07-07 7:10 PM
[webinar - Program decision trees in sensors with a Machine Learning Core]
Solved! Go to Solution.
2020-07-07 7:11 PM
Technically every board which mounts an ST device having the MLC capability is able to run and execute MLC-based algorithms. Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on the ST device through any hardware or development board (e.g. through firmware upgrade).
Regarding the STEVAL-STWINKT1, we are working to add an official support to STWIN on our software tools, to simplify the process. The target is to have the STWIN fully supported by our tools in Q3.
2020-07-07 7:11 PM
Technically every board which mounts an ST device having the MLC capability is able to run and execute MLC-based algorithms. Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on the ST device through any hardware or development board (e.g. through firmware upgrade).
Regarding the STEVAL-STWINKT1, we are working to add an official support to STWIN on our software tools, to simplify the process. The target is to have the STWIN fully supported by our tools in Q3.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.