2020-07-07 7:15 PM
[webinar - Program decision trees in sensors with a Machine Learning Core]
Solved! Go to Solution.
2020-07-07 7:16 PM
Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.
A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.
2020-07-07 7:16 PM
Except for the SensorTile.box, NUCLEO-F401RE, NUCLEO-L476RG with expansion boards X-NUCLEO-IKS01A2 or X-NUCLEO-IKS01A3 and SensorTile are directly supported in AlgoBuilder.
A custom HW can be also used. For custom hardware it is necessary to create an AlgoBuilder firmware template using STM32CubeMX and X-CUBE-ALGOBUILD extension.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.