2025-01-09 9:38 PM
I am working on ism330dlc to find gyroscope x, y, and z values. I am getting x, y, and z values. I am also getting variable x, y, and z values when the board is maintained constant. I wrote registers are 0x1204,0x1160,0x1060,0X22,0X23,0X24,0X25,0X26, and 0X27. Pleas
Solved! Go to Solution.
2025-01-10 12:23 AM
Hi @Saikumar_avantel ,
Can you share a screenshot and the log file of the acquired data?
Thanks!
2025-01-10 12:23 AM
Hi @Saikumar_avantel ,
Can you share a screenshot and the log file of the acquired data?
Thanks!
2025-01-10 1:26 AM
I'm not using the controller. I'm using FPGA.
2025-01-10 1:29 AM
Ok, but can I see this variation in the output? Which is the order of magnitude?
2025-01-10 1:30 AM
The spi clock is 1MHz, and the delay between commands is 10 milliseconds. I don't have stored values, but if you want the source, I can share it.
2025-01-10 1:32 AM
what do mean about magnitude?
2025-01-13 1:15 AM
yes, it could be useful to understand the variation!
2025-01-15 9:12 PM
What do u mean magnitude ? isn't ODR ?
are please provide sequence list of registers to get GYRO data from ISM330dlc
2025-01-15 10:13 PM
if it is possible to offer technical support (such as Skype or Microsoft Teams). I'll show you my screen so you can help me figure out what's wrong.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.