2020-04-12 9:38 AM
Hello everyone,
I'm trying to do the PDM-PCM transformation of MP3DT05 microphone data in a STM32L433RC nucleo board. For my understanding, the better is to use an existing library... But I don't know which one I could use, and I can't even find any practical example.
The application notes available are not helping. I'm receiving the PDM data through HAl_SAI_DMA_receive.
I hope someone can help me find the right way to do this.
Thank you
2020-04-16 1:45 AM
Hi @ALope.1 , I would suggest you to start from an existing reference design platform mounting an STM32L4xx device and a digital microphone, equipped with the proper acquisition libraries (via I2S peripheral and PDM-PCM conversion). The reference function pack for ST MEMS microphones is the X-CUBE-MEMSMIC1, and the NUCLEO board closest to STM32L433 could be the STM32L476RG-Nucleo with the digital audio stream acquisition demonstration. You can find the project example in \Projects\STM32L476RG-Nucleo\Demonstration\CCA02M2\Microphones_Streaming. Regards
2020-04-16 7:56 AM
Hi @ALope.1
You can refer to PDM library : STM32Cube_FW_L4_V1.15.1\Projects\STM32L4R9I-EVAL\Demonstrations\STemWin\MB1315\Modules\audio_player\Addons\PDM
it may help you to implement your application.
Best regards
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.