2020-07-23 2:31 AM
Hi, i want to use VL53L1X and VL53L3CX to detect a small size target (e.g finger,rope) at 1 meter away. i am wandering what's the minimum target size for VL53L1X and VL53L3CX ?
Thanks.
2020-07-23 2:39 AM
Hi
A finger at 1 m will be difficult to detect, actually the surface is too small and the distance is too long to have enough photons coming back even if the human skill has a quite good IR refelectance ~60%. Anyway, you have better chance with the L1X and the L3CX because the L1X has lens so better sensitivity. Just try it.
Thanks,
Julien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.