2021-11-24 11:51 AM
I have both these devices on the same I2C bus and am trying to calculate the maximum pullup resistance.
Thanks!
Solved! Go to Solution.
2021-11-26 7:36 AM
Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.
Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.
\Tom
2021-11-26 7:36 AM
Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.
Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.
\Tom
2022-08-17 12:15 PM
Hello All!
Is it possible to interrogate 30 sensors through the I2C expander without using an interrupt
- LIS2MDL ? I can attach the diagram in the next message if necessary.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.